SSP (SPI) Frame Timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SSP (SPI) Frame Timing

861件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TahaSN on Fri Jan 03 15:07:30 MST 2014
Hello,

I am using LPC4350 (Hitex Board A4) and using SSP in SPI Mode with SCL Frequency of 20 MHz. I am trying to get data from the slave but I noticed that the time between each frame is quite a lot (around 20us) which doesn't suite my application. I tried using interrupts as well but the time doesn't change that much. The frame size is 16 bits so the whole frame should take around 1us but I dont know where other 18-19us are wasted at. Does anybody have a clue? Am I missing something?

Taha
ラベル(1)
0 件の賞賛
返信
0 返答(返信)