SPIFI with LPCXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPIFI with LPCXpresso

1,366 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jschuld on Wed May 08 21:59:14 MST 2013

Hi,


We are in the process of developing a board with the LPC4333. We have all the peripherals working well, but like to move from the SPI interfcae to the SPIFI interface. I am trying to locate some example projects which use the SPIFI interface that work with LPCXpresso (the development environmend we use). I have found some that are for Keil uVision, but not for LPCXpresso.


On that note, I'm also looking for a development board which has some working example code for the SPIFI with ideally a LPC43xx device. I have used the EA 4088 development board before, which does come with a device connected to SPIFI, but there is only example code available for uVision for SPIFI.


Any recommendations are welcome,


Regards,


J.

Labels (1)
0 Kudos
Reply
0 Replies