SPIFI vs SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPIFI vs SPI

2,611 Views
TEMCEFF
Contributor IV

What is difference between  Interfacing of External Serial flash using SPIFI and SPI? what are the Advantages of using SPIFI over SPI?

Labels (1)
0 Kudos
Reply
1 Reply

2,461 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Muralidhar,

The SPIFI focuses on interface with SPI flash only, the SPI is an interface which can connect to a lot device including flash.

Regarding the difference, the normal SPI module has 4 signals: /SS, SCLK, MOSI and MISO signals, the /SS, SCLK and MOSI are driven by SPI master, the MISO signal is driven by slave. The normal SPI can interface with single I/O SPI flash.

The SPIFI interface includes /SS, SCLK and dual/quad/8 data lines, the data lines are bidirectional, they can input or output. In general, the Data0 line is command line, it transfer command to flash in the first phase, then the spifi module transfers address by all data lines or just data0 line, then spifi can transfer data depending on the command.

The SPIFI can generate the timing to access spi flash.

I attach the RM of SPI flash, pls refer to the doc to know the required timing of spi flash.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply