SPI1 address incorrect in the manual

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI1 address incorrect in the manual

1,421 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc_bloke on Mon Jun 02 09:25:55 MST 2014
Hi all,

While working on the LPC800 chip I have discovered an error in the User Manual.

'Table 203. Register overview: SPI (base address 0x4005 8000 (SPI0) and 0x4008 C000
(SPI1))' Page 236 of UM10601 v1.6

The address for SPI1 should infact be 0x4005 C000

This while a small issue did indeed have me wondering when I was trying to debug an issue with SPI1.

Otherwise I love the chip it is great.

标签 (1)
0 项奖励
回复
3 回复数

1,412 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpc_bloke on Thu Oct 09 06:40:16 MST 2014
It does indeed mean that the SOIC20 only has 1 SPI interface where as the TSOP20 has 2 SPI interfaces.  I'm speaking for first had experience here, you have to be careful which chip you select.

I felt when I figured out what was going on and investigated the number is SPI blocks.  It is correctly documented and the problem is clearly mine.
0 项奖励
回复

1,412 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Wed Oct 08 11:48:39 MST 2014
In the data sheet it says:

Quote:
Remark: SPI0 is available on all LPC800 parts. SPI1 is available on parts
LPC812M101JDH16 and LPC812M101JDH20 only.



Does that really mean that there is no SPI1 on LPC812M101JD20 ?
Even though the pinout is the same as the LPC812M101JDH20?

0 项奖励
回复

1,412 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Thu Jun 05 14:00:51 MST 2014
Hi,

Thank you. It was indeed a typo . We will fix it.

Thanks,
NXP Technical Support
0 项奖励
回复