SGPIO camera interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGPIO camera interface

3,802件の閲覧回数
dimitrissideris
Contributor III

Is there any LPCOpen SGPIO camera example except from AN11343?

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

3,380件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Dimitris,

We have no other LPCOpen example but here is another application note:

http://cache.nxp.com/documents/application_note/AN11196.zip

Or this one that uses the SCT to interface with the camera:

http://cache.nxp.com/assets/documents/data/en/application-notes/AN11365.pdf 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

3,380件の閲覧回数
maneesh_pawar
Contributor I

I am unable to locate the project files and code used in the Application Note http://cache.nxp.com/assets/documents/data/en/application-notes/AN11365.pdf

Can you please share it.

Regards

0 件の賞賛
返信

3,380件の閲覧回数
dimitrissideris
Contributor III

Thanks for the reply Carlos.

Yes i have checked the application notes you mentioned above.

Although they are useful, they all are for Keil boards.

I though maybe there is some lpcxrpresso lpcopen sgpio examples so that i can use them as base for my implementation.

I wonder why lpcopen examples don't have at all any spgio periph example

0 件の賞賛
返信

3,380件の閲覧回数
dimitrissideris
Contributor III

I would like some help for the an11343 example code implementation.

The example is a dual core M0-M4 implementation.

The SGPIO interrupt handler lies inside M0 example code and it handles the sgpio interrupts. The slice and pin configuration of sgpio lie in M4 example code. Ok straight forward.

I see that in M4 example code there is a Gpio interrupt handler which is actually the VSYNC interrupt hanlder. (Vsync is connected to gpio pin not sgpio).

// GPIO IRQ slot 6 is used by VSync IRQ, common to all cameras
void ATR_RAMCODE GPIO6_IRQHandler(void)
{
    LPC_GPIO_PIN_INT_Type *pPinInt = LPC_GPIO_PIN_INT;    
    // leave M0 to process GPIO6 int
    if (pPinInt->RISE & BVON(PIQ_VSYNC))
    {
        // rising edge
        // previous frame is completed
        pPinInt->RISE = BVON(PIQ_VSYNC);
        NVIC_DisableIRQ(SGPIO_IINT_IRQn);
        SGPStop();
        s_ccb.vsyncCnt++;
        // judge whether is the previous frame is received        
        if (s_ccb.sgpIntPerFra != 0)
        {
            __set_PRIMASK(1);
            s_ccb.rdyRxBufCnt++;
            #if 0 == IS_TWIN_RXBUF
            #else
            s_ccb.rcvTglBit ^= 1;
            #endif            
            __set_PRIMASK(0);
            s_ccb.vsyncEffCnt++;            
            s_ccb.sgpIrqCntInPrevFra = s_ccb.sgpIntPerFra;            
        }
        s_ccb.sgpIntPerFra = 0;
        if (s_ccb.freeRxBufCnt)
        
            s_ccb.freeRxBufCnt--;            
            #if 0 == IS_TWIN_RXBUF
                s_ccb.pBuf = s_ccb.pRcvDbBuf->aa32[0];
            #else
                s_ccb.pBuf = s_ccb.pRcvDbBuf->aa32[s_ccb.rcvTglBit];
            #endif
            s_ccb.pBufEnd = s_ccb.pBuf + (CAP_BUF_SIZE / 4);
            SGPGetRdyToGo();
        
                __sev();
        }        
    }

There is some comment " // leave M0 to process GPIO6 int".

Is this true;

If not and comments are wrong,

sgpio interrupt hander is in M0 code and gpio handler for vsync is in M0?

0 件の賞賛
返信

3,380件の閲覧回数
dimitrissideris
Contributor III

Also in M0 example code of AN11343 there are two sgpio interrupt handlers.

void ATR_RAMCODE SGPIO_IRQHandler(void)

void SGPIO_IRQHandlerB (void)

Why is that for?

0 件の賞賛
返信