I am trying to configure my AS4C2M32SA-6TIN 64MB SDRAM on my LPC4337 (costum board).
I have verified that the EMC clock is half M4 core clock (204/2=102MHz) but when measuring A0
this is only running at 1MHz (expected to run at half core clock when read/write to the entire SDRAM).
What could be the reason for this? I got an MPC4357-EVB with 32MB 16-bit SDRAM and got the example working in uVision.
When trying to use this example on my 64MB 32-bit SDRAM in emIDE (with corrected parameters that fits this SDRAM) nothing works.
my config setup can be seen here http://pastebin.com/WAu4hXke
Hope someone is able to help.