Running code on LPC4330 from internal SRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running code on LPC4330 from internal SRAM

1,137 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kris_sin on Sun Feb 16 17:02:20 MST 2014
Hi guys,

I am using latest LPCXpresso 6.14 with LPCXplorer4330. So far I have run my application on SPIFI Flash but now I wanted run the code from RAM. Can someone help configure linker script, startup file to make the code run from internal SRAM? If someone has modified some basic blinky example that runs from SRAM I would realyy appreciate haring it with me and all forum viewers.
Labels (1)
0 Kudos
Reply
1 Reply

1,077 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Feb 17 05:05:26 MST 2014
Please don't post the same question more than once. I've posted a response in the other thread that you created.

http://www.lpcware.com/content/forum/running-code-ram#comment-1135347

Regards,
LPCXpresso Support
0 Kudos
Reply