Resources for getting Azure GUIX running on the lpc55s28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Resources for getting Azure GUIX running on the lpc55s28

1,622 Views
hsabro
Contributor I

I'm currently evaluating whether I can use the Azure GUIX module as a graphics library on the LPC55S28. My system is already running Azure RTOS threadx and USBX.

I've been trying to find resources and/or examples on getting the GUIX part running, but no success so far. The SDK management doesn't seem to be able to provide a working library either, missing "ports".

Is the GUIX portion not yet supported on this device, or am I missing something? Any help or pointers appreciated.

0 Kudos
Reply
2 Replies

1,582 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the SDK of LPC55xx just ports the basic part of Azure RTOS threadx, but does not port the GUIX module.

For the GUI, the LVGL tools is supported for LPC family, I suggest you use LVGL tools.

This is the LVGL tools website:

https://www.nxp.com/design/software/embedded-software/lvgl-open-source-graphics-library:LITTLEVGL-OP...

 

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

1,567 Views
hsabro
Contributor I

Thanks for your input. I guess that's a little bit disappointing given the SDK builder claims GUIX is supported on this device, but it does answer my question at least. So, really, it's "not supported".

I'll have a look at the LVGL solution then.

0 Kudos
Reply