Replacement of SWM(Switch Matrix) in LPC55s69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Replacement of SWM(Switch Matrix) in LPC55s69

1,333件の閲覧回数
ravicha
Contributor II

i have code for LPC804 of UART1 and UART2 where UART1 is responsible for communication to the smart card and UART2 is for genrating the clock for smart card , this two UART used throught SWM 

now i want to replace this in lpc55s69 how to do it

1 返信

1,298件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @ravicha 

USART functions are available on all LPC55S6x/LPC55S2x/LPC552x devices as a
selectable function in each Flexcomm Interface peripheral. Up to 8 Flexcomm Interfaces
are available. So you can choose two of them to use.

 

BR

Alice

0 件の賞賛
返信