Reading and Writing USB Flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reading and Writing USB Flash memory

1,874件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aclgn on Wed Jun 18 01:02:30 MST 2014
Hi,i use LPC17XX and i have questions ,thanks for your answers.
firstly,i want to Read a usb momory card ,actually i wanna Read a .txt file or .hex file or.log file on usb momory and 
secondly, i wanna Write  text file to usb momory from getting on uart
but i dont know how can i began ?
can you give a suggestion for me?
how can i  start?
can i use USB library ?and  how can i read and write text or onother file from usb  memory?

ラベル(1)
  • USB

0 件の賞賛
返信
2 返答(返信)

1,858件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by keemi on Sat Oct 11 00:20:55 MST 2014
its very good post
0 件の賞賛
返信

1,858件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Jun 20 10:47:36 MST 2014
Hi,

Have you tried the LPC17xx USBdevice MSC example ?

visit : http://www.lpcware.com/content/nxpfile/lpc177x-and-lpc178x-cmsis-compliant-standard-peripheral-firmw...

Also refer to the Dual-Hi Speed Application note .

visit : http://www.lpcware.com/content/project/Dual-USB-Host-Device-solution


Thanks,

NXP Technical support
0 件の賞賛
返信