RS232 interface with full modem signals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RS232 interface with full modem signals

1,443件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wafa on Wed Jan 16 01:01:26 MST 2013
I'm using the LPC1788 processor, and am working with USB_VirtualCom example. It works fine with UART0 but not with UART1 (TX:P3.16,RX:P3.17), i need to make it work with UART1 and not UART2 because my out is the RS232 interface and i want it to be with all modem signals wich it's possible with UART1 only.Help please.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,419件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Nov 06 04:37:32 MST 2014
Deleted -- I did not notice the age of the OP [Today's reply looks like spam]
0 件の賞賛
返信

1,419件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shineandlive124 on Thu Nov 06 01:07:30 MST 2014
Good day! Thank you for posting this is one I really appreciate it! I will surely be back here for more updates!
Anyways check this out to,  <a href="http://buildmylikes.org/followers/">gain instagram followers</a>
0 件の賞賛
返信