Proteus : Gives error for my first example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Proteus : Gives error for my first example

1,688件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PrakashPrasad on Wed Apr 02 02:00:00 MST 2014
Below is my code for which I have generated the hex file:



#include "lpc214x.h"



#define LED1    (1 << 10)

#define LED2    (1 << 11)

#define BUTTON1 (1 << 15)

#define BUTTON2 (1 << 16)



// Method prototypes

int getPinState(int pinNumber);



int main(void)

{

  // Set buttons as input

  PINSEL0 &= ~(BUTTON1 | BUTTON2);



  // Set LEDs as output

  PINSEL0 |= (LED1 | LED2);



  // Turn both LEDS off (set them 'high')

  IO0SET |= (LED1 | LED2);



  while (1)

  {

    // Check if button 1 is pressed

    // Released = 'High' (1)

    // Pressed =  'Low'  (1)

    if (getPinState(15))

    {

      // Button1 is currently 'high'

      // Turn LED1 off

      IO0SET |= LED1;

    }

    else

    {

      // Button1 is currently 'Low'

      // Turn LED1 on

      IO0CLR |= LED1;

    }

  }

}



int getPinState(int pinNumber)

{

  // Read the current state of all pins in GPIO block 0

  int pinBlockState = IO0PIN;

  // Read the value of 'pinNumber'

  int pinState = (pinBlockState & (1 << pinNumber)) ? 1 : 0;

  // Return the value of pinState

  return pinState;

}



Also attached is my PROTEUS simulation model. But in PROTEUS I am getting error?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)