Program JN5179 with JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program JN5179 with JTAG

6,357件の閲覧回数
fricart
Contributor I

Hi,

I want to avoid mount the FT230XS chip in the final design. Can I program the JN5179 Flash via JTAG (with LPC-Link2)?

Thank you,

Fer.

タグ(2)
0 件の賞賛
返信
6 返答(返信)

6,031件の閲覧回数
wupengfei
Contributor II

 Can you tell me how JN5179 is going into programming mode? I follow the instructions of the technician SPIMIMO-> GND,RESET-GND,VDD->3.3V still can not recognize the JN5179 device. Thank you.

6,031件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Wu Pengfei.

Be sure the next two points

1 The JN517x will enter UART programming mode if SPIMISO (DO1) pin 24 is low after RESET.

2 The JN517x will enter JTAG programming mode if SPICLK (DO0) pin 23 is low after RESET.

Note: The DO0 must be left floating high during reset to avoid entering JTAG programming mode

Regards,

Mario

6,023件の閲覧回数
Irfan2
Contributor I

Hello Sir,

 

I am also facing the issue in Programming.

 

When I make DO1 to low by shorting it to the GND then LPCexpresso not able to detect even JN5179 IC.

 

Also even after programming connection it is get heated as well.

 

We have used the DO1/SPIMISO pin to the external flash as MISO and for Boot to put the controller in programming mode.

 

Let me your suggestion to make it in programming mode and resolve the issue.

 

 

Thanks,

Mahammadirfan Saiyed

0 件の賞賛
返信

5,989件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

When I make DO1 to low by shorting it to the GND then LPCexpresso not able to detect even JN5179 IC.

Try to let the pin floating when you try to program the device.

Note: The JN5179 is not recommended for the new designs and it is nor supported. I recommend the JN5189 instead.

Regards,

Mario

0 件の賞賛
返信

6,031件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Fernando,

Yes. You can program the JN5179 Flash via JTAG (with LPC LINK2).

Please see the JN517x LPCXpresso Installation and User Guide 

2.3 Loading an Application into a JN517x Device

http://cache.nxp.com/documents/user_manual/JN-UG-3109.pdf?fsrch=1&sr=3&pageNum=1 

Best Regards,

Mario

0 件の賞賛
返信

6,031件の閲覧回数
fricart
Contributor I

Thank you Mario for the response. I'm going to review that document.

Best Regards,

Fer.

0 件の賞賛
返信