Product Selector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Product Selector

2,626 Views
dingelen
Contributor III

I'm searching an MCU, preferably from the LPC family to start a new development. After using the product selector for some time, it wondered me that I was always getting a very limitted number of hits. https://www.nxp.com/parametricSearch#/category/c731_c380_c732

The reason as it seems that this list is full of holes and missing data. Example the LPC154x will show as having no USB. And similar errors are found all over this table. This is very inconvenient to use as a search tool.

Is there an excel somewhere which is complete? And ranges all the relevant parameters? (Core, Temp, USB, Package, Price, Flash, RAM, EEPROM,...)

0 Kudos
Reply
1 Reply

2,460 Views
soledad
NXP Employee
NXP Employee

Hi, 

Thank you for your feedback, please check the following document and let me know if this helps, 

https://www.nxp.com/docs/en/product-selector-guide/LPCMICROLNCD.pdf

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply