Product Info LPC2368FBD100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Product Info LPC2368FBD100

1,896 Views
AFZ
Contributor I

Hi,

we are using "LPC2368FBD100" in our board. i would like to know some development board that has this type of microcontroller.

this product is available or it is going obsolete , if yes, what is the alternative ?

may i use the supercap with VBAT pin instead of using battery ?

Thanks

 

Regards

Afz

0 Kudos
Reply
3 Replies

1,889 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Recommend you choose other product ,you see this chip remains in longevity program until 2022,

also this is old part, almost not available. 

Please tell us your requirement, then we can give you some suggestion.

 

BR

Alice

0 Kudos
Reply

1,884 Views
AFZ
Contributor I

Hi,

 

can you please suggest an alternative ?

we prefer same footprint with almost same pin order.

same price list.

Thanks.

 

 

 

0 Kudos
Reply

1,878 Views
frank_m
Senior Contributor III

AFAIK, the LPC17xx controllers are mostly pin compatible to the LPC23xx. Which would be the LPC1768 in your case.

However, aside from alleged recent shortages, this series is not much younger than the LPC23xx, and might not save you for long.

0 Kudos
Reply