Problems with forum posting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with forum posting

1,411件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rickta59 on Sun Oct 20 09:25:07 MST 2013
I've tried to follow up to my lpc1114-community-where-it thread 3 times. My posts just keep disappearing. Where do they go? Are they being moderated or is there just problems with the forum software?

-rick
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,405件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rickta59 on Sun Oct 20 11:58:23 MST 2013
Thanks, if you want to delete this post that would be great... it would also be great if you could delete this one:

http://www.lpcware.com/content/forum/lpc1114-community-where-it#comment-1132850

as it is a duplicate.

Thanks again,

-rick
0 件の賞賛
返信

1,405件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Oct 20 11:39:48 MST 2013
Your posts were getting spam trapped for some reason. And at weekends I'm afraid that the spam traps are checked less frequently. I have now released all your posts though.

Anyway, I'm not sure why you were getting spam trapped - possibly a combination of an external link that the spam trap software didn't like, following by multiple almost identical posts in a certain time frame.  Anyway, I'll pass this issue on to the site admin team for investigation.

Regards,
LPCXpresso Support
0 件の賞賛
返信