Problem to read a with lpcopen (LPC1837)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem to read a with lpcopen (LPC1837)

829 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by goffi on Mon Jul 21 08:03:11 MST 2014
I'm trying to read the sandisk sdcard i found in the evaluation board.

Using the latest lpcopen, when i read a sector (no matter which) ,my buffer is filled with only zeros (cid, csd are ok and no errors during the commands). Using the same program, i can read an unbranded sdcard and it works very nice.

The sample (dual device) works also with the sandisk card, but the libraries are different and is impossible to do some comparing.

Who can help me?
Thanks
Labels (1)
0 Kudos
Reply
0 Replies