Problem 16 bit tft configuration in LPC1788

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem 16 bit tft configuration in LPC1788

1,085 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aaram on Thu Feb 06 22:52:30 MST 2014
Hi to all,

I have configured 7 inches tft LCD with LPC1788 controller for 24 bit and it is working without any problem. but now i need to reconfigure it to 16bit. So I changed the value of BPP in LCD control register to 6 from 5. Now the letters and all the shapes in tft lcd got bigger(doubled).

When iam using 24bit in LCD I was using two hynix sdram of  size 16Mx16 each. Now i reduced it to one. But stil it is not working. Can someone please me on this issue........

SDRAM CONFIGURATION:


#define DYN_CONTROL_NOP_COMMAND0x00000183
#define DYN_CONTROL_PALL_COMMAND0x00000103
#define DYN_CONTROL_MODE_COMMAND 0x00000083
#define DYN_CONTROL_NORMAL_COMMAND 0x00000000

#define EMC_CLOCK      60000000
#define NANO_SEC       (1/1000000000) 

#define NS_TO_CLKS(ns) ( (uint32_t)( (double)(ns) * EMC_CLOCK * NANO_SEC ) + 1 )


#define SDRAM_BASE_ADDRESS      0xA0000000   /* CS0 */

#define REFRESH_TIME_MAX 0X7FF

void sdram_initialization (void){

unsigned long Dummy;
  LPC_SC->PCONP |= (1<<11); 

emc_sdram_pin_allocation ();

LPC_SC->EMCDLYCTL = 0x00080808;   

  EMC_CONTROL = 0x00000001;
  EMC_CONFIG  = 0x00000000;  

LPC_SC->EMCCLKSEL=0;    //60 MHZ

EMC_DYN_REFERESH    = REFRESH_TIME_MAX;/*260 usec*/
EMC_DYN_RASCAS0    = 0X00000303;
EMC_DYN_READ_CONFIG = 0x00000001; /* Command delayed strategy, using EMCCLKDELAY */
  
  EMC_DYN_RP         = NS_TO_CLKS(18);
  EMC_DYN_RAS        = NS_TO_CLKS(42);
  EMC_DYN_SREX       = 1;
  EMC_DYN_APR        = 1;
  EMC_DYN_DAL        = 2+NS_TO_CLKS(18);
  EMC_DYN_WR         = 1;
EMC_DYN_RC         = NS_TO_CLKS(63);
EMC_DYN_RFC        = 4;
  EMC_DYN_XSR        = 1;
  EMC_DYN_RRD        = NS_TO_CLKS(15);
  EMC_DYN_MRD        = 2;

EMC_DYN_CONFIG0   =  (1<<10) | (1<<9) | (1<<7);/* 256Mb, 16Mx16, 4 banks, row=13, column=9, RBC */\


  EMC_DYN_CONTROL    = DYN_CONTROL_NOP_COMMAND;
  delay_in_millisecond(100);  /* wait 100ms */

  EMC_DYN_CONTROL    = DYN_CONTROL_PALL_COMMAND;
delay_in_millisecond(500);

  EMC_DYN_REFERESH    = NS_TO_CLKS(7812)>>4;  //30   64ms/8192=7812 nsec

  EMC_DYN_CONTROL    = DYN_CONTROL_MODE_COMMAND;
Dummy = *((volatile uint32_t *)(SDRAM_BASE_ADDRESS | (0x33<<12)));
delay_in_millisecond(100);
  EMC_DYN_CONTROL    = DYN_CONTROL_NORMAL_COMMAND;

  EMC_DYN_CONFIG0 |= 0x80000; /* enable buffer */
delay_in_millisecond(100);
}



7 INCHES TFT LCD CONFIGURATION:

#define TFT_H_SIZE           800
#define TFT_H_PULSE          2
#define TFT_H_FRONTPORCH     17
#define TFT_H_BACKPORCH      45

#define TFT_V_SIZE           480
#define TFT_V_PULSE          2
#define TFT_V_FRONTPORCH     22
#define TFT_V_BACKPORCH      22

#define LCD_EN (1<<0)
#define BPP     6
#define LCDTFT (1<<5)
#define BGR    (1<<8)
#define LCDPWR (1<<11)
#define IVS    (1<<11)
#define IHS    (1<<12)
#define BCD    (1<<26)

void glcd_initialization (){

unsigned long i;
unsigned long *pDst = (unsigned long *)LCD_VRAM_BASE_ADDR;
  
//  IOCON_P0_4   = LCD_RED;
//IOCON_P0_5   = LCD_RED; 
// IOCON_P4_28  = LCD_RED;
IOCON_P4_29  = LCD_RED;
IOCON_P2_6   = LCD_RED; 
IOCON_P2_7   = LCD_RED; 
IOCON_P2_8   = LCD_RED; 
IOCON_P2_9   = LCD_RED;
  
// IOCON_P0_6   = LCD_GREEN; 
// IOCON_P0_7   = LCD_GREEN;
IOCON_P1_20  = LCD_GREEN; 
IOCON_P1_21  = LCD_GREEN; 
IOCON_P1_22  = LCD_GREEN; 
IOCON_P1_23  = LCD_GREEN; 
IOCON_P1_24  = LCD_GREEN; 
IOCON_P1_25  = LCD_GREEN;

// IOCON_P0_8   = LCD_BLUE ; 
// IOCON_P0_9   = LCD_BLUE ; 
// IOCON_P2_12  = LCD_BLUE ;
IOCON_P2_13  = LCD_BLUE ;
IOCON_P1_26  = LCD_BLUE ; 
IOCON_P1_27  = LCD_BLUE ; 
IOCON_P1_28  = LCD_BLUE ; 
IOCON_P1_29  = LCD_BLUE ;

IOCON_P2_2   = LCD_DCLK ;
IOCON_P2_5   = LCD_HSYNC;
IOCON_P2_3   = LCD_VSYNC;
IOCON_P2_4   = LCD_LCDDEN;
IOCON_P2_0   = LCD_PWR; 

LPC_SC->PCONP |= 1<<0;

LCD_CTRL_REG &= 0;
LCD_CTRL_REG |= (BPP<<1)|LCDTFT;
LCD_CTRL_REG &= ~BGR;
LCD_CTRL_REG &= ~LCDPWR;

LCD_POL_REG &= 0;
LCD_POL_REG |=(5<<0)|1<<6;
LCD_POL_REG |=IVS|IHS|BCD;
LCD_POL_REG |= (TFT_H_SIZE-1)<<16;
LCD_POL_REG |=(0<<27);

LPC_SC->LCD_CFG = 7 ;// 120000000 / ((unsigned long) C_GLCD_PIX_CLK); 15 MHZ

/*Refresh time 41msec*/

LCD_TIMH_REG  &= 0;
LCD_TIMH_REG |= (TFT_H_BACKPORCH - 1)<<24;
LCD_TIMH_REG |= (TFT_H_FRONTPORCH - 1)<<16;
LCD_TIMH_REG |= (TFT_H_PULSE - 1)<<8;
LCD_TIMH_REG |= ((TFT_H_SIZE/16) - 1)<<2;


LCD_TIMV_REG  &= 0; 
LCD_TIMV_REG |= (TFT_V_BACKPORCH)<<24;
LCD_TIMV_REG |= (TFT_V_FRONTPORCH)<<16;
LCD_TIMV_REG |= (TFT_V_PULSE - 1)<<10;
LCD_TIMV_REG |= TFT_V_SIZE - 1;

LCD_UPBASE_REG = LCD_VRAM_BASE_ADDR & ~7UL ;
LCD_LPBASE_REG = LCD_VRAM_BASE_ADDR & ~7UL ; 

for( i = 0; (TFT_H_SIZE * TFT_V_SIZE) > i; i++)
  *pDst++ = White;

  for(i = 10000; i; i--);

//LCD_CTRL_REG |= LCDPWR| LCD_EN;
LCD_CTRL_REG |= LCDPWR;//| LCD_EN;
}

void lcd_powerenable(){

LCD_CTRL_REG |= LCD_EN;
}

void lcd_powerdisable(){

LCD_CTRL_REG &= LCD_EN;
}
Labels (1)
0 Kudos
Reply
0 Replies