Persistent across power cycles variable storage with LPC54018 single SPI Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Persistent across power cycles variable storage with LPC54018 single SPI Flash

1,238 Views
mitchkapa
Contributor III
Hi,
 
I'm using an LPC54S018 microcontroller with a 16 MB SPIFI flash.  The application code is too large to fit into RAM and so I am using the XIP_IMAGE flag during compile.  I need to store variables in the flash for access across power cycles.  I have been following the steps listed in this forum post:
 
but I can't modify the "test" variable once the code is running, because it is read-only.  Is there a way to make the test variable read/write, and able to be saved across power cycles?
 
Thanks for your help,
Mitch
0 Kudos
Reply
1 Reply

1,212 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI mitchkapa 

If you want variable read/write, we must store it in RAM.

If you store it in SPIFI Flash, please refer spifi_dma_transfer or spifi_polling_transfer demo code in SDK folder to program the related address.

Thanks,

Jun Zhang

0 Kudos
Reply