PN5180 HCET4T ported library to custom LPC1769

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN5180 HCET4T ported library to custom LPC1769

1,361 次查看
tsotnek
Contributor II

Hello,

 

 

I have a PNEV5180 eval board and I am porting the HCE example 8 T4T library to a custom LPC1769 board that I have designed. I currently have a problem though, in phacDiscLoop_Run after autocoll occurs and after I read data from PN5180 Rx Buffer, the RF_STATUS{RF_DET_STATUS} is then being set to 0. I tested with the actual PNEV5180 board and it's still set to 1. Could anyone from NXP tell me what could be the possible problem?

 

Thanks

0 项奖励
回复
1 回复

1,325 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi tsotnek:

Could you please provide more information about your question?

what does "the RF_STATUS{RF_DET_STATUS} is then being set to 0" mean? 

 

Regards

Daniel

0 项奖励
回复