OpenOCD support for LPC55S69 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenOCD support for LPC55S69 EVK

4,276 Views
cgarcia
Contributor II

Is there OpenOCD support for LPC55S69 EVK board ? based on CMSIS-DAP probe

Labels (1)
0 Kudos
Reply
5 Replies

4,267 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cgarcia,

This is belongs to 3rd party. We never declaim we support OpenOCD.  I suggest you using the MCUXpresso IDE associating with the JLINK or CMSIS DAP interface to download the code.


OpenOCD can support many company MCUs, The supported chips are listed there.

http://openocd.org/

 

BR

Alice

0 Kudos
Reply

4,258 Views
cgarcia
Contributor II

Hi Alice,

Thanks for replaying, yes MCUXpresso IDE is a good option however I am working in a project that support multiple vendors and a generic open tool is a good option to keep common environment.

I think just I have to find a proper LPC55S69 config file for openocd, if you know someone from community has worked about it, please let me know.

Thanks  

0 Kudos
Reply

2,985 Views
Aisha
Contributor I

Hey , 

I am working on the same project as you were , can you tell me how much did you progress ahead and the basic procedure with which you accessed LPC55sx family using openocd?

0 Kudos
Reply

4,254 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cgarcia,

I searched the community , also talking internal with my other  colleague, we haven't meet customer use this as so far, sorry for the inconvenient .

 

BR

Alice

0 Kudos
Reply

4,250 Views
cgarcia
Contributor II

Alice,

I haven't found something about it neither, thanks I appreciate your help.

Thank you.

0 Kudos
Reply