OpenOCD support for LPC55S69 EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenOCD support for LPC55S69 EVK

4,264件の閲覧回数
cgarcia
Contributor II

Is there OpenOCD support for LPC55S69 EVK board ? based on CMSIS-DAP probe

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

4,255件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cgarcia,

This is belongs to 3rd party. We never declaim we support OpenOCD.  I suggest you using the MCUXpresso IDE associating with the JLINK or CMSIS DAP interface to download the code.


OpenOCD can support many company MCUs, The supported chips are listed there.

http://openocd.org/

 

BR

Alice

0 件の賞賛
返信

4,246件の閲覧回数
cgarcia
Contributor II

Hi Alice,

Thanks for replaying, yes MCUXpresso IDE is a good option however I am working in a project that support multiple vendors and a generic open tool is a good option to keep common environment.

I think just I have to find a proper LPC55S69 config file for openocd, if you know someone from community has worked about it, please let me know.

Thanks  

0 件の賞賛
返信

2,973件の閲覧回数
Aisha
Contributor I

Hey , 

I am working on the same project as you were , can you tell me how much did you progress ahead and the basic procedure with which you accessed LPC55sx family using openocd?

0 件の賞賛
返信

4,242件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello cgarcia,

I searched the community , also talking internal with my other  colleague, we haven't meet customer use this as so far, sorry for the inconvenient .

 

BR

Alice

0 件の賞賛
返信

4,238件の閲覧回数
cgarcia
Contributor II

Alice,

I haven't found something about it neither, thanks I appreciate your help.

Thank you.

0 件の賞賛
返信