OM13092/J14 expansion header's SPI interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13092/J14 expansion header's SPI interface

900 Views
belmontbob59
Contributor IV

I am confused about the documentation. It reads:

pastedImage_1.png

This does not mention JS34 or JS35 for FC3's MISO/MOSI However the schematic has this for J14:

pastedImage_4.png

and this for the MCU:

pastedImage_2.png

And this:

pastedImage_3.png

So by default the MCU FC3's MISO/MOSI pins are routed to the SDRAM correct? This means that I can not use J14 extension header FC3. But the documentation (table 14 just above) does not mention to modify JS34 and JS35. Further more the table "JS33, JS34,JS35,JS36"  reads to shunt JS34/JS35 in position 2-3 (default) when using 3.3V.

So does this means that the expansion port J14 can not be used? 

Please advise

Labels (1)
0 Kudos
Reply
0 Replies