hello. I am using an OM13054 (LPC-Link 2) board and flashing the firmware using the ARM 20-10 JTAG Connector.
The firmware flash tool uses the built-in Flash tool in MCUXpresso IDE :)
However, when I run debug for testing, I get an unexpected error.
The OM13054 (lpc-link-2) board is connected to the PC via micro USB.
Here are the errors:
Unable to connect wire for probe index 1.
Error: Wire Ack Fault - target connected?
For more information about the error, I have attached a photo. Please check the attached file.
Do you have any guides on how to solve this problem??
解決済! 解決策の投稿を見る。
To update LPC-Link2 with LPCscrypt
If CMSIS-DAP interface can't be connect with IDE, try Jlink interface,
Thanks,
Jun Zhang
Hi
When you use LPC-Link2 debug a target, Could you please check in windows manager if LPC-Link2 is correctly recognized?
Not sure if on board LPC-Link2 firmware is damaged, Please try to update LPC-Link2 firmware with LPCScrypt for either CMSIS-DAP and Jlink . can it update successfully? ( Note, all ensure that jumper JP1 is NOT fitted so that the probe will be DFU bootable at power on. after the firmware update, remove JP1, power off and power on)
https://www.nxp.com/design/microcontrollers-developer-resources/lpcscrypt-v2-1-2:LPCSCRYPT
Best Regards
Jun Zhang
To update LPC-Link2 with LPCscrypt
If CMSIS-DAP interface can't be connect with IDE, try Jlink interface,
Thanks,
Jun Zhang
Thank you sir. Now problem is solved!