Number of PCLK cycles for CT32Bn_MAT0 pin to change state when a match occurs between the TC and MR0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Number of PCLK cycles for CT32Bn_MAT0 pin to change state when a match occurs between the TC and MR0

628 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abasak on Fri Mar 11 02:17:17 MST 2016
Hello,

This is with reference to LPC111x series of uC (specifically LPC1114FN28). My question is how many number of PCLK cycles does it have to elapse for CT32Bn_MAT0 pin to change state when a match occurs between the TC and MR0?

In case the timer is configured to generate an interrupt on match, the manual says that interrupt indicating that a match occurred is generated in the next clock after the timer reached the match value. Is it the same for changing the state of CT32Bn_MAT0 pin?

Thanks!
Abhishek

标签 (1)
0 项奖励
回复
1 回复

611 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复