Not compatible emulators available - LPC4088 developer's kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not compatible emulators available - LPC4088 developer's kit

2,306件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by loveyjspark on Sun Apr 17 17:31:59 MST 2016
Hello~

I use belows
H/W : the LPC4088 developer's kit
IDE : LPCXpresso 8.1.4(Free Edition)

I executed 'periph_blinky' example on the LPCXpresso
and then I executed Debug 'periph_blinky'
but a dialog was up on the screen with this messages.
There were no emulators.
(I just connected to host computer with a usb cable and heard start melody.)

Connect to emulator: NXP LPC40xx
No compatible emulators available.
They may be disconnected, not powered, already in use or not compatible with this target

please give me some tips which can connect with my LPC4088 devloper's kit.

Thank you for your consideration
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,229件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

2,229件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 18 00:33:12 MST 2016
If you are referring to this kit ...

https://www.embeddedartists.com/products/kits/lpc4088_kit.php

then I don't believe it has a built in debug probe. So you will need to connect via an external probe, such as as LPC-Link2. For more information, please see the LPCXpresso User Guide - as provided within the product, or the following FAQ:

https://www.lpcware.com/content/faq/lpcxpresso/supported-debug-probes-mcus

Regards,
LPCXpresso Support
0 件の賞賛
返信

2,229件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by loveyjspark on Sun Apr 17 22:20:17 MST 2016
lpc-link2 has to use to download lpcopen programs like 'periph_blinky' on the LPC4088 developer's kit?
I'm a totally beginer in the nxp.
please help me.
0 件の賞賛
返信