No such file or directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No such file or directory

309 Views
chuandaoxy
Contributor I

I'm compiling lpc810 code by  MCUXpresso IDE v11.5.1 ,The compilation result is shown in Fig

chuandaoxy_0-1716111953495.png

#include <core_cmInstr.h> It's already been added,anyone tell me where the path should be added

thank you

0 Kudos
Reply
1 Reply

269 Views
HangZhang
NXP Employee
NXP Employee

Hi @chuandaoxy,

You need to add the path of the core_cmInstr. h file to the project settings of MCUXpress IDE v11.5.1. The specific operation steps are as follows:

1 Open MCU Xpress IDE v11.5.1.
2 In the Project Browser, right-click on your project and select "Properties".
3 In the pop-up properties window, select "C/C++Build" ->"Settings" ->"MCU Settings" ->"Include Paths".
4 Click the "Add" button, then enter the path where the core_cmInstr. h file is located in the pop-up dialog box, and click "OK".
5 Click the "Apply" button, then click the "Close" button to close the properties window.
Recompile the project.
In this way, the path to the core_cmInstr. h file has been added to the project, and it should be found during compilation.

Hope this will help you.

BR

Hang

0 Kudos
Reply