No GUI Files Error while creating a library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

No GUI Files Error while creating a library

2,042 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mohammadyou on Sat May 30 20:57:52 MST 2015
Hi all.
based on the DOC I want to create a library so I copied the makefile.bat and the others requirements (prep.bat - CC.bat - Lib.bat from 'ARM-IAR' Folder) to the root directory (inside 'start' folder of 'emWin BSP') and Edited the Prep.bat and point it to the folder of IAR Toolpath  I face a problem same as below. before clicking closing the CMD Window the 'Temp' and 'Lib' folder is created but after that it's gone!!
would you please tell me what the problem ?
[img=630x377]http://www.lpcware.com/system/files/1_0.png[/img]
标签 (1)
0 项奖励
回复
0 回复数