New project with LPC18XX or LPC43XX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

New project with LPC18XX or LPC43XX

952件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ennio on Thu Nov 28 09:31:38 MST 2013
Dear LPCware forum,
I have to develop very fast a new family of machines and I have to chose a new microprocessor.
I think that NXP could be the best choise.
I would like to know if it is possible to have with the LPC18XX family or the LPC4XXX family the following resources at the same time?

-) n°4 UART

-) n°3 SPI

-) n°16 ADC

-) n°12 PWM

-) n°1 DAC

-) SD card

-) USB



Let me know!



Best regards
ラベル(1)
0 件の賞賛
返信
1 返信

925件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Nov 29 01:17:50 MST 2013
I see someone has already posted a response on this question in your duplicate post…

http://www.lpcware.com/content/forum/new-project-lpc18xx

Please don't post the same question multiple times!

0 件の賞賛
返信