Net-snmp 5.4.3 error at the time of installation for porting into linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Net-snmp 5.4.3 error at the time of installation for porting into linux

1,423 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MOHAMMAD BIYABANI on Thu Mar 21 21:50:26 MST 2013
Hi,
I am Trying to install NET-SNMP 5.4.3 but getting the errors.The problem is when i was installed NET-SNMP then it is showing

../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_register_null_context'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_register_null'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_get_bulk_to_next_handler'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_register_old_api'
../agent/.libs/libnetsnmpagent.so: undefined reference to `netsnmp_init_helpers'
collect2: ld returned 1 exit status
make[1]: *** [snmptrapd] Error 1
make[1]: Leaving directory `/home/mohan/net-snmp-5.4.3/apps'
make: *** [subdirs] Error 1

Initially it was also shown the
/usr/bin/ld: cannot find -lperl error
But that was rectified by installing libperl-dev package. I have tried to rectify remaining two errors but the problem has not solved.
I attached the snap shot of error message also it is useful to give answer.

Thanks & Regards,

MOHAMMAD BIYABANI.
Labels (1)
0 Kudos
Reply
0 Replies