Need sample code for interfacing a 8.4" TFT LCD display to LPC1788

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need sample code for interfacing a 8.4" TFT LCD display to LPC1788

1,384 Views
kevinvalentine
Contributor I

The display is a Kyocera T-55786GD084J

0 Kudos
Reply
1 Reply

1,264 Views
soledad
NXP Employee
NXP Employee

Hello Kevin,

Unfortunately we don't have an example for this display, however you can  check the below application note that you can use as reference. 

http://www.nxp.com/documents/software/AN11206.zip 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply