Need help for IAR EWARM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help for IAR EWARM

1,288 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andyyau on Sun May 26 10:10:23 MST 2013

Hi,


I am new to LPC and staring IAR EWARM. It is not easy to get information of the following:


1. How to create a brand new project with CMSIS support for LPC1114? I cannot find any code template for it.


2. Where is the LPC1114 peripheral drivers of for ADC, UART, Timer...?


3. I tried LPCopen drivers, but my EWARM versoin is 6.4. When I open the project, it will get error as 6.5.2 is required. Any way to fix this?


Thanks a lot!


Andy

Labels (1)
0 Kudos
Reply
1 Reply

1,277 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Mon Jun 03 10:05:00 MST 2013

There will be an IAR verison of the project guide (similar to the Xpresso project guide) for the next version of LPCOpen. However, you can get information on needed files, include paths, etc. from the current Xpresso version of the project guide @ http://docs.lpcware.com/lpcopen/v1.03/_l_p_c_o_p_e_n__x_p_r_e_s_s_o__p_r_o_j_e_c_t__p_o_r_t_i_n_g__g...


http://www.lpcware.com/content/project/lpcopen-platform-nxp-lpc-microcontrollers/lpcopen-upcoming-re...

0 Kudos
Reply