Need BSDL files for LPC55S28JBD100 and PLX2162PC82029B/LX2162RE82029B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need BSDL files for LPC55S28JBD100 and PLX2162PC82029B/LX2162RE82029B

3,346 Views
pmuppala
Contributor I

I am working on test development for a board with LPC55S28JBD100 SoC and PLX2162PC82029B(ES part number)/LX2162RE82029B(production part number). We are planning to use JTAG boundary scan since both devices are boundary scan complaint.

It would also be great if you can provide information on how to set each device into boundary scan mode. 

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

3,248 Views
HeMyFAE
NXP Employee
NXP Employee

Dear Sabina,

the BSDL file that we downloaded for LPC55s28 seems to be incorrect.

It shows that it has 200+pins .

The most the LPC55sxx has is 100 pin.

REgards,

hy

0 Kudos
Reply

3,250 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hope you are well. This has been posted yesterday.

LPC55 series BSDL files 

From our team:

The BSDL file is include all pins information for the die of LPC55Sxx.

But, only valid pins on LQFP or VFBGA  package can be used for BSDL test tools, for example, JTAG Live.

User may ignore the rest of un-used pins.

Best Regards,

Sabina

0 Kudos
Reply

3,251 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

For the LPC55S28JBD100 please visit out microcontroller symbols. footprints and models page. Here you will find the files that are available. For the BSDL file you will have to request it. You will find a link to fill out the form.

For the PLX2162, please contact your distributor or direct sales representative as this part is not yet publicly available. 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply