NXP USB Stack Licence agreement copy for LPC1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP USB Stack Licence agreement copy for LPC1788

1,566件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jay123 on Thu Jun 26 01:07:09 MST 2014
please share USB Stack licence agreement copy for LPC1788 microcontroller

i'm using LPC USBLib.
USB Class Use: CDC
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,513件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Jul 08 02:57:50 MST 2014
You should not reuse a defined vid/pid for another use - it will cause many driver problems. You should get one of your own. See
http://www.lpcware.com/content/project/usb-vid-pid-program
0 件の賞賛
返信

1,513件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jay123 on Tue Jul 08 01:37:43 MST 2014
waiting for reply....................
0 件の賞賛
返信

1,513件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jay123 on Thu Jun 26 22:05:59 MST 2014
i have used NXP VCOM demo code but disable serial port for data transmission.
i'm using this for application downloading and keep VID and PID ID same as VCOM.

Use of Application:
1) Connect USB to computer and computer will generate COM port
2) user can select virtual COM port No. ( Disable baudrate,parity and stopbit selection because serial port is disable for data transmission)
3) now user can download application through selected port mention in step 2.

Can i use same PID for my appliaction or i need to register for new PID?
0 件の賞賛
返信