NXP Smartphone Quick-Jack compatility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Smartphone Quick-Jack compatility

1,581 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Sat Jan 31 08:07:18 MST 2015
Hi,

I am sure this has been asked before but I cannot find any definitive answer.

Is the NXP Smartphone Quick-Jack card compatible with a Samsung Galaxy Tab 3 model SM-T210R

Thanks in advance for any help.

JOhnR
Labels (1)
0 Kudos
Reply
3 Replies

1,562 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JoelEkstein on Thu May 05 00:53:26 MST 2016
I would refer my extended warranty when this happens, A replacement would be better.
0 Kudos
Reply

1,562 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Sat Jan 31 15:50:24 MST 2015
Hi,

Thanks for replying

I had already read Chapter 8 of AN11552.pdf

Quote:

Quick-Jack has been tested and verified to work on the following devices:
• iOS: iPhone 4, iPhone 4S, iPhone 5 and iPhone 5S (iOS 6.1.6 and iOS 7.0.4).
• Android: Samsung Galaxy S3.
Compatibility with other iOS/Android devices is not guaranteed. This chapter gives a short overview why there may be compatibility issues, and gives hints how these may be resolved


and

Quote:

Therefore, the Quick-Jack Android compatibility is limited to the Samsung Galaxy S3. Other Android phones may work, but certain properties of the current hardware/software are known to limit the number of supported Android phones


I guess my question should have read "Has anybody used the NXP Quick-Jack board with a Galaxy Tab 3 tablet?"

JohnR
0 Kudos
Reply

1,562 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sat Jan 31 12:37:03 MST 2015
Read chapter 8 of the app note...
http://www.nxp.com/documents/application_note/AN11552.pdf
0 Kudos
Reply