[NHS 3100] Error on debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[NHS 3100] Error on debugging

1,572件の閲覧回数
rado__99
Contributor II

Hello, I face the following problem when I am in debugging mode and tap a NFC reader over the board.

Redlink interface error when debugging:255

I am using the dpu_templogger example with debug build downloaded on the board.

Thank you in advance.

0 件の賞賛
返信
1 返信

1,506件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Is it the dp_tlogger example or the one for UCODE? and which IDE are you working with?

Thank you.

Regards,

Ivan.

0 件の賞賛
返信