[NHS 3100] Error on debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[NHS 3100] Error on debugging

1,572 Views
rado__99
Contributor II

Hello, I face the following problem when I am in debugging mode and tap a NFC reader over the board.

Redlink interface error when debugging:255

I am using the dpu_templogger example with debug build downloaded on the board.

Thank you in advance.

0 Kudos
Reply
1 Reply

1,506 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Is it the dp_tlogger example or the one for UCODE? and which IDE are you working with?

Thank you.

Regards,

Ivan.

0 Kudos
Reply