Mouse cursor moves automatically

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mouse cursor moves automatically

3,125件の閲覧回数
FreKa
Contributor I

Hello, I do my first steps with LPCExpresso55S69. When I connect the USB cable of the LPCExpresso55S69 board to my notebook and the demo program starts running, the mouse pointer automatically moves in a rectangle on the screen. If I plugged the USB cable out, the cursor stopps. Who can help in this problem ? What can I do ?

0 件の賞賛
返信
3 返答(返信)

3,112件の閲覧回数
ErichStyger
Specialist I

do not plug in the board on the device USB port. Use the debug USB (label Debug Link) port instead.

0 件の賞賛
返信

3,119件の閲覧回数
ErichStyger
Specialist I

That's probable the USB HID (Mouse) program running on that board. The demo emulates a mouse and moves the cursor in a rectangle around.

0 件の賞賛
返信

3,116件の閲覧回数
FreKa
Contributor I
Ok, I thought the demo programme only concerned the LED and the buttons. How can I stop it so that I can load my own programmes ? When the cursor is moving it is hardly possible.
0 件の賞賛
返信