Minor error in documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minor error in documentation

1,778 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xander.houtman on Wed Mar 18 03:55:52 MST 2015
Hello LPC community,

I found a minor error in the User manual for the LPC175x/6x series (UM10360).

On page 62, in the description of the PCON register, bit 3 and 4 are defined twice. Once related to brown-out and once as reserved.

I assume the brown-out version is correct.

Link to document:
http://www.nxp.com/documents/user_manual/UM10360.pdf
Labels (1)
0 Kudos
Reply
3 Replies

1,767 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Mar 18 09:12:22 MST 2015
Hi xander.houtman,

I see the documentation error now. :)

This will be reported to the documentation team. Thank you for letting us know!
0 Kudos
Reply

1,767 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xander.houtman on Wed Mar 18 08:00:15 MST 2015
A minor miscommunication.

The reserved bits after bit 4 range from 3 to 7, which should be 5 to 7.
0 Kudos
Reply

1,767 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Mar 18 07:25:02 MST 2015
Hi xander.houtman,

I opened the link you provided and went to page 62 and do not see that bit 3 and bit 4 are identical. Bit 3 is able to turn off all of the brown-out circuitry while bit 4 will disable the brown-out reset but does not disable a brown-out interrupt.
0 Kudos
Reply