Memory space problem LPC1114/333

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory space problem LPC1114/333

1,896 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ALERICO90 on Fri Jul 10 06:24:52 MST 2015
Hello I hace a problem with my LPC1114/333, this LPC has 56K flash memory but I only can flash near 32K of the memory not even close to 56K.. what can I do?, I put the correct devive on keil uvision and still I can't flas more than 32K. Here is a screen capture of my target options
Labels (1)
0 Kudos
Reply
1 Reply

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Jul 10 14:49:46 MST 2015
Hi,

Please check the flash drivers used in Utilites->Settings. The Flash driver should be 56 Kb  i.e. LPC1xxx_56.FLM.

Thanks
NXP Technical Support
0 Kudos
Reply