Maximum Input Frequency of LPC81x?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum Input Frequency of LPC81x?

1,439件の閲覧回数
tiberiumcode
Contributor I

I'm trying to make a high frequency counter out of an LPC81x. I can use an external crystal to make the LPC81x run at 24 MHz, but I'd like to count the frequencies of square waves in the 100MHz-200MHz range. Can I configure the SCT and its prescalers to count faster than the bus clock, or do I need to use a clock divider chip external to the LPC81x? I cannot find the dynamic characteristics of the microcontroller's inputs in either the UM10601 LPC81x User Manual or the LPC81x datasheet.

0 件の賞賛
返信
1 返信

1,369件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Daniel Vibbert 

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, the duration of the high and low levels on the input pin must be greater than 1 clock cycle, and the frequency of the input must be less than one-quarter of the clock rate.
About your question, the LPC81x is incapable of detecting the input PWM whose frequency exceeds the 100 MHz.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信