MCUXpresso patch libraries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso patch libraries

1,619 Views
bjorns
Contributor III

Hello,

I'm using MCUXpresso to generate code and to include libraries etc needed for the project. However I need to patch one of the libraries (in this case fatfs to add another driver). As soon as I regenerate the project the patched files are overwritten. Is there any elegant way of handling this or should I give up and make a copy of fatfs that I can manage myself?

Thanks
/Björn

Labels (1)
0 Kudos
Reply
1 Reply

1,593 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello bjorns,

The configuration files for pins, clocks and peripherals are fully generated by the config tools. The user should use MCUXPresso config tools user interface to make any changes and the re-generate the code. It’s not supported to do manual changes in the generated files.

 

 

BR

Alice

0 Kudos
Reply