MCUXpresso IDE JLink Debugger launch config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE JLink Debugger launch config

Jump to solution
1,637 Views
robberpen
Contributor III

Hi

I study debug tool on MCUXpresso IDE User Guide. and interesting about Debug seting "SEGGER Jlink" below. But I have no idea how to lanuch Dailog from instruction below.

What is "lauch config file"?

image.png

0 Kudos
Reply
1 Solution
1,596 Views
Alex_Wang
NXP Employee
NXP Employee

Hi, @robberpen 

The "launch config file" is a configuration file that is used to set and configure the parameters of a debugger such as SEGGER Jlink at startup. This file usually contains information about the target device to which the debugger is connected, debugging interface Settings, and so on.

Alex_Wang_0-1712887351726.jpeg

Best regards, Alex

 

View solution in original post

0 Kudos
Reply
1 Reply
1,597 Views
Alex_Wang
NXP Employee
NXP Employee

Hi, @robberpen 

The "launch config file" is a configuration file that is used to set and configure the parameters of a debugger such as SEGGER Jlink at startup. This file usually contains information about the target device to which the debugger is connected, debugging interface Settings, and so on.

Alex_Wang_0-1712887351726.jpeg

Best regards, Alex

 

0 Kudos
Reply