MCUExpresso and ea LPC1788 tcpecho sample

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUExpresso and ea LPC1788 tcpecho sample

1,945件の閲覧回数
vbravosalazar
Contributor I

Hello there,

I was wondering is anybody has experienced problems trying to debug the sample tcpecho_freertos sample. I have successfully imported the project and the necessary board and chip  support into an MCUExpresso Workspace. I can build and download it to the Embedded Artists LPC1788 dev but I cannot run debug it without crashing at the network interface initialization (netinf). 

However, if I reset the board after the crash I can see the example running. At this point, I can ping the address I assigned it and I can  attach the debugger. Any points here?

Thanks,

Vladimir

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,809件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Which MCUXpresso IDE version do you have?

Which OS do you have? 

does it happen with the other LPCOpen examples?

Could you please try to create a new workspace and import your projects into the new workspace.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信