MCU-LINK-PRO VCOM Voltage Range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU-LINK-PRO VCOM Voltage Range

1,320件の閲覧回数
LuisC
Contributor II

Hello,

I just wanted to get a clear answer on whether the VCOM port of the MCU-LINK-PRO Debug Probe can operate at both 3.3V and 1.8V. From the RM, I see that the SPI, I2C and triggering digital signals of the J19 header can be in the range of 1.2V-5.5V. However, I couldn't find any voltage specs for VCOM.

 

If it is able to receive and transmit UART data at 1.8V (assuming 3.3V is default), do I need to make any modifications (removing jumpers, etc...) for it to work?

0 件の賞賛
返信
1 返信

1,309件の閲覧回数
ErichStyger
Specialist I

See the schematics:

ErichStyger_0-1687798416108.pngErichStyger_0-1687798416108.png

But be aware that the other UART pins are directly connected to the MCU (3.3V):

ErichStyger_1-1687798509050.pngErichStyger_1-1687798509050.png

 

 

I hope this helps,

Erich

0 件の賞賛
返信