MCB4300 blinky binary image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCB4300 blinky binary image

1,710件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Sat Feb 08 06:06:25 MST 2014
Dear members,

I'm new to LPC4300. I'm using LPC21, LPC17, LPC11, LPC8 already. But right now I'm not yet fit enough to create even a simple blinky program for a LPC4300, because I don't have a development environment set up.
I'm still at the step of updating my flash programmer to support LPC4300, and this is a major update, because of the flash bank challange. So I need an absolutely reliable binary that I can use for testing, that easily shows some activity (like for example LED flashing) on this board?

Would anyone of you be so kind to provide me with one (*.bin, *.hex)?
I have a Keil MCB4300 with that row of 8 LEDs (P0.10..P0.14, P9.0..P9.2) below the LCD.
In return, I would provide my Linux flash utility  ;-)

Thanks in advance!

By the way, who is using Linux for programming the LPC4300 and who isn't even using an IDE?
What tools do you use for flashing it?
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,668件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Mon Apr 28 18:25:11 MST 2014
It took some time and considerable effort to keep my promise. Here it is:

mxli-3.0
0 件の賞賛
返信

1,668件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Sat Feb 08 09:52:05 MST 2014
Wow! Thanks a lot, Alex!

It works! Some Knight-Rider-style of a running light  :)

At first, I forgot to set active bank to A (didn't know it's necessary), but now it's working.
0 件の賞賛
返信

1,669件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by abb on Sat Feb 08 09:14:18 MST 2014
Hello Marc,

I've built two HEX files from C:\Keil\ARM\Boards\Keil\MCB4300\Blinky project with UV4 for you. LPC4357-Flash-A-Blinky_FlashA.hex works on my Keil MCB4357 board.

Best regards,
Alex
0 件の賞賛
返信