MBEDTLS 4.x Port for LPC55S28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MBEDTLS 4.x Port for LPC55S28

Jump to solution
428 Views
guitardenver
Contributor IV

I was wondering if NXP has an example using the latest MBEDTLS 4.x with the LPC55S28. The SDK downloads seem to have MBEDTLS3.x. Is there an example using/porting MBEDTLS 4.x to use the LPC55S28 hardware accelerators?  Or even a 4.X example with a similar MCU?

I do not need TLS. Just basic PSA crypto portion of the new 4.X version. 

- AES-CCM

- HKDF-SHA256

-SHA256

-HMAC-SHA256

Labels (1)
0 Kudos
Reply
1 Solution
388 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @guitardenver 

Currently, NXP does not provide a public example of Mbed TLS 4.x (TF‑PSA‑Crypto) running on LPC55S28 with hardware acceleration. The MCUXpresso SDK still mainly uses Mbed TLS 3.x, and the available PSA crypto examples are also based on 3.x rather than 4.x.

mbedtls3x_examples — MCUXpresso SDK Documentation

BR

Harry

View solution in original post

0 Kudos
Reply
1 Reply
389 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @guitardenver 

Currently, NXP does not provide a public example of Mbed TLS 4.x (TF‑PSA‑Crypto) running on LPC55S28 with hardware acceleration. The MCUXpresso SDK still mainly uses Mbed TLS 3.x, and the available PSA crypto examples are also based on 3.x rather than 4.x.

mbedtls3x_examples — MCUXpresso SDK Documentation

BR

Harry

0 Kudos
Reply