LwIP FreeRTOS TCPECHO client code issues!!!!!1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LwIP FreeRTOS TCPECHO client code issues!!!!!1

1,713件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aastha001 on Thu Apr 30 03:36:42 MST 2015
iam currently working LPCOPEN with LwIP on LPC1830...i tired to ping with example code  of TCPECHO which is in server mode with remote host ...successfully pinging as per my applicationplatform i modified as a client code ...i tired all possbility to send a dummy data by using netconn_write to the remote host which is running on linux server socket programming....but iam unable to succedd by this way   if attaching my code if anybody can help me out to complete my project to be vy gratfeul for u to proceed further...
ラベル(1)
0 件の賞賛
返信
0 返答(返信)