LWIP Don`t work, hard fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LWIP Don`t work, hard fault

1,280 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ezequiel on Tue Mar 26 04:56:02 MST 2013
hi,

I'm trying to run the lwIP library in LCP1788 MCU and the KSZ8041 PHY.

I'm trying to run the example tcp_eco no operating system.

The problem is as follows:
While not connect the ethernet cable running the firmware.But when I connect the cable to a PC, hard fault is generated.

The hard-fault error happens in the lpc_low_level_input function line 414

/* Free pbuf from desriptor */
lpc_enetif->rxb[idx] = NULL; <-- Hard fault on this!!!
lpc_enetif->rx_free_descs++;

Here I detail the result of the debug for both cases.

With the ethernet cable connected:


sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sys_timeout: 20005028 msecs=5000 handler=arp_timer arg=00000000
netif_set_ipaddr: netif address being changed
netif: IP address of interface netif: netmask of interface netif: GW address of interface netif: added interface en IP addr 192.168.0.44 netmask 255.255.255.0 gw 10.1.10.1
netif: setting default interface en
tcp_bind: bind to port 25


Without the ethernet cable connected:


sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sys_timeout: 20005028 msecs=5000 handler=arp_timer arg=00000000
netif_set_ipaddr: netif address being changed
netif: IP address of interface netif: netmask of interface netif: GW address of interface netif: added interface en IP addr 192.168.0.44 netmask 255.255.255.0 gw 10.1.10.1
netif: setting default interface en
tcp_bind: bind to port 25
sct calling h=ip_reass_timer arg=00000000
tcpip: ip_reass_tmr()
sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sct calling h=ip_reass_timer arg=00000000
tcpip: ip_reass_tmr()
sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sct calling h=ip_reass_timer arg=00000000
tcpip: ip_reass_tmr()
sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sct calling h=ip_reass_timer arg=00000000
tcpip: ip_reass_tmr()
sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sct calling h=arp_timer arg=00000000
tcpip: etharp_tmr()
etharp_timer
sys_timeout: 20005028 msecs=5000 handler=arp_timer arg=00000000
sct calling h=ip_reass_timer arg=00000000
tcpip: ip_reass_tmr()
sys_timeout: 2000503c msecs=1000 handler=ip_reass_timer arg=00000000
sct calling h=ip_reass_timer arg=00000000
tcpip: ip_reass_tmr()
sys_timeout: 2000503c msecs=1000 handler=
.
.
.
.
.

I expect a prompt response,
regards,
Ezequiel Picca.
Labels (1)
0 Kudos
Reply
0 Replies