LPCopen example project cannot compile

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCopen example project cannot compile

2,841 次查看
Laxmi_Gangal
Contributor I

I am using keil uvision 4, and trying to use keil_uvision_projects projects from lpc open.

Without changing any settings however, if I just try to load for  the periph_can project found at

lpcopen_2_07_keil_iar_nxp_lpcxpresso_1769\applications\lpc17xx_40xx\keil_uvision_projects\nxp_lpcxpresso_1769\periph\periph_can

When I compile I get this message:

.\keil_output\iflash_nxp_lpcxpresso_1769\can_iflash_nxp_lpcxpresso_1769.axf: error: L6002U: Could not open file ..\..\..\..\..\..\software\lpc_core\lpc_board\boards_17xx\nxp_lpcxpresso_1769\keil_output\board_nxp_lpcxpresso_1769.lib: No such file or directory

 

Then I tried this wrt my project,

1.Go to        "C:\lpcopen_2_10_keil_iar_ea_devkit_1788\software\lpc_core\lpc_board\boards_17xx\ea_devkit_1788"
2.Open "lib_lpc_board_ea_devkit_1788.uvproj"
3.Build this project (now keil made board_ea_devkit_1788.lib")

 

then also i am getting this error

.\keil_output\iflash_nxp_lpcxpresso_1769\can_iflash_nxp_lpcxpresso_1769.axf: error: L6002U: Could not open file ..\..\..\..\..\..\software\lpc_core\lpc_board\boards_17xx\nxp_lpcxpresso_1769\keil_output\board_nxp_lpcxpresso_1769.lib: No such file or directory

 

For which I can find no reason, because having inspected the directory, the file .lib is present there there.

Any help much appreciated
Labels:
LPCOpen

标签 (1)
0 项奖励
回复
2 回复数

2,822 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Laxmi_Gangal 

Please import chip and board lib projects, and build them. Then compile example project. 

If still have issue, please take a video or screenshot show your detail steps. 

 

BR

Alice

0 项奖励
回复

2,806 次查看
Laxmi_Gangal
Contributor I

yes i imported the files then also i am getting this error. please help me to resolve this.

0 项奖励
回复